1/5/2008 1:37 PM | |
Joined: 4/6/2006 Last visit: 2/5/2024 Posts: 604 Rating:
|
Hello Late, I've received that update too but it seems the download is not available yet. S7-Distributed Safety V5.4 + Service Pack 4 |
Best regards, |
|
1/5/2008 2:27 PM | |
Joined: 1/7/2006 Last visit: 3/9/2025 Posts: 2705 Rating:
|
Hi, I have seen (and mentioned) that. Also the FM352/452 package is given free for upgrading to VISTA Configuration Package for Cam Control FM 352 FM 452 V6.0 And SINEMA E is now also given free with version SINEMA E 2006 + SP2.... Service Pack 2 for SINEMA E 2006 Released for Delivery That have the advantage under VISTA that you didn't need a external card like the CP 7515, there is a new driver built in the package for site surveys. Changes of the Site-Survey function (measuring of WLANs)
I will place all the update links in thestart of this thread.... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/6/2008 9:02 PM | |
Joined: 1/7/2006 Last visit: 3/9/2025 Posts: 2705 Rating:
|
Hi, I have tested the package for SINEMA E and also for the FMx52, both are working fine. Also the next package is given free and is installed by me, it works fine. ET 200S 1SI Serial Interface Function Blocks, Examples and User Manuals for the ET200S 1SI Serial Interface DS V5.4 SP4 is still not downloadable.... maybe next week. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
1/8/2008 8:17 AM | |
Joined: 9/28/2005 Last visit: 10/24/2024 Posts: 414 Rating:
|
Hi Late, Thanks for all the testing. I've got a new challenge for you: S7-GRAPH V5.3 SP5. Could you give STEP5 V7.23 also a try? And ProTool V6.0 SP3? |
Smurf |
|
1/8/2008 9:45 PM | |
Joined: 1/7/2006 Last visit: 3/9/2025 Posts: 2705 Rating:
|
Hi Schlumpf, Because S7 Graph V5.3 SP5 is higher then the one I have tested it is automatically given free... I'm afraid that packages that are not in the actif catalog anymore won't be given free on VISTA.... |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on