10/22/2018 12:44 PM | |
Posts: 7 Rating:
|
Hello, am sorry to wake up old topic, but I have similar problem. After adding new module to configuration, a can't compile without errors or warnings. In diagnostic buffer I get these error: I/O access error, reading P area, word access, Access address: 328 Request OB: I/O access error OB (OB122) Priority class 1 External error, Incoming event If I compile project I get these: Compile: VERSO_1_22102018\SIMATIC 300 Station\CPU 315-2 DP\S7 Program\Blocks -> Object compilation was executed (with warnings) Warning: The S7 program contains the following blocks that are referenced but not available: FC1, FC7, FC12, FC23, FC35 Date: 10/22/2018 time: 12:40:08 PM Compile: VERSO_1_22102018\SIMATIC 300 Station\CPU 315-2 DP\Connections -> Object was compiled without errors I have attached the project, I'm doing this as my home project, Thank you all already for help! Simon AttachmentVerso_1_.zip (163 Downloads) |
Follow us on