5/8/2019 1:14 PM | |
Joined: 3/17/2013 Last visit: 7/15/2024 Posts: 481 Rating:
|
Hi We have WCIII Robicon VFD. Recently tank level went low due to water leak from one of the cell hoses at inlet start point . Fault logs are attached herewith. Part of SOP is as below In the drive SOP it is being generated by INTERNAL FLAG $TankHighLevel = UserFault44_O; UserFault44Wn_O = TRUE; TankHighLevel = InternalNetInFlag35_I; UserText44 = "Coolant Tank High"; My question is why the drive should read tank level high, while it tripped on Tank low low/ MV TRAFO OT (over temperature) Regards, N Vijay AttachmentFault Log 5-7-2019 20-54_txt .pdf (260 Downloads) |
Follow us on