8/15/2016 7:32 AM | |
Joined: 6/1/2016 Last visit: 6/3/2023 Posts: 29 Rating:
|
Dear Expert and PCS7 Users. I also have a problem with Wed View Publisher in Wed Navigator of PCS7 V8.1 Attached file is what i got when tried to Publish screens. i used PCS7 8.1 and this can work normally in Window 7 prof but display this error message in Window server. I don;t know this problem come from installed software mismatch or some missing setting. Does anybody got this problem? could you please share how to fix it. Much appreciate for your attention. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/15/2016 1:52:00 PMNew subject after splitting |
|
8/16/2016 4:20 PM | |
Posts: 111 Rating:
|
Hello ND120685, as far as I understand the pictures, there is a mismatch with the data of your objects. The first error messages says that properties were deleted which have had a reference to no more available objects. The logfile says that: - properties of some objects were deleted e.g. second error message "DataSet1:Double0" - the deleted properties was bounded to some Typicals properties e.g. property "Text" in @PCS7TypicalsBasisLibraryv8.PDL @@SFC_TPYE/2 The error message and log file say that the properties must be rebounded. Perhaps the there are some objects which aren't available (e.g. deleted)or needs to be published too? Is there a dismatch between objects/ porject on the Win7 PS and the Win Server? I don't know the exact solution, but perhaps the translation of message and log file may help you. Additional information which may help: https://support.industry.siemens.com/cs/ww/de/view/109736233/en 2.3.3.5 Web Publishing Wizard 2.4.2.2 Configure the WinCC project https://support.industry.siemens.com/cs/ww/de/view/109485959/en 8.1.3 requirement for web publishing |
This contribution was helpful to
1 thankful Users |
Follow us on