1/8/2020 9:30 AM | |
Posts: 162 Rating: (8) |
To be noticed: you can not mount/detach backups (if you want to use old segments of trend or alarm archive). |
This contribution was helpful to1 thankful Users |
1/8/2020 9:41 AM | |
Joined: 11/15/2015 Last visit: 5/18/2024 Posts: 179 Rating: (28) |
Dear MrcCristian A web client is always a bit slower than a normal RT client, but the difference is only marginal, and you only notice it when you switch directly from an RT client to a web client. Depending on what you use for a function in your WinCC projects, you have to note that not all options e.g. in C script can also be used on the web navigator. Standard functions like masking a few bits here and there or doing calculations with variables are no problem.
|
Look for alternative not for the correct answer...if this is helping you rate it. |
|
This contribution was helpful to1 thankful Users |
Follow us on