11/23/2015 5:04 PM | |
Posts: 124 Rating: (4) |
try this please: s7-1200 and s7-1500 webserver step by step trends |
11/23/2015 5:16 PM | |
Joined: 7/1/2014 Last visit: 7/2/2024 Posts: 230 Rating: (25) |
That would be useful if the images for coding were not so little... and i don't see any attachment to this article (i expected a file with the example described)... :( |
11/23/2015 6:40 PM | |
Posts: 124 Rating: (4) |
you should add and download three javascript library: 1. jquery-1.11.3.min.js and jquery-2.1.4.min.js 2. jquery.flot.js and jquery.flot.time.js
3. Moment.js describing: Flot is a javascript plotting library, it`s small, performance is good and supports all kinds of chart types. There are also plugins for Flot to use. Moment.js is a free and open source JavaScript library that removes the need to use the native JavaScript |
Last edited by: saleh at: 11/23/2015 6:45:58 PM |
|
11/24/2015 3:08 PM | |
Joined: 7/1/2014 Last visit: 7/2/2024 Posts: 230 Rating: (25) |
Ok so the jquery for the javascript functionality, jquery flot for the graph and moment to manage the "date" more easily? The image you attacched is too little... :) |
11/24/2015 3:42 PM | |
Posts: 124 Rating: (4) |
yes. I attached image that token from this link: s7-1200 and s7-1500 webserver step by step trends this image say: you must use some java script library. this is very simple |
Last edited by: saleh at: 11/24/2015 3:44:03 PM |
|
11/24/2015 4:55 PM | |
Joined: 7/1/2014 Last visit: 7/2/2024 Posts: 230 Rating: (25) |
That is what i understood from that "tutorial"
But i think there is something wrong... maybe some parentesis... if i understand right when it's ok, i should see a line of the value that is datalogged... after i manage to make this work i will need to find out how to have multiple values. |
1/16/2018 11:49 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by grabekradek is split to a separate thread with the subject Separate data into individual columns in CSV. Best regards |
Follow us on