1/19/2020 3:00 PM | |
Joined: 1/6/2011 Last visit: 8/29/2024 Posts: 45 Rating:
|
[snip] But Now there is different type problem. This 421 has a load cell under a bin which is loaded with material using a conveyer. We load 1000kg of material and start loading on it. The weight displayed also increases gradually as it fills and reaches 1000kg correctly. Then withing 1-2 seconds it shows 0kg. But the material is still in the bin. Basically it does not remains at 1000kg. what could be the problem now? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/20/2020 11:59:19New subject after splitting. Division of questions into separate topics. |
|
Follow us on