8/1/2019 2:32 PM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Please also see the attached screenshots. I have a newly installed WinCC 7.4 Upd1 server (installed on a Windows server 2012 R2). I have set the IP addresses as they should be in the Windows server 2012 R2 and I have connected the server to a simple switch (temporarily - to download the project). I have set PG/PC to TCP.1 on the netcard I am thinking I am using (2 netcards in the Windows server). I have set the correct IP address on my Engineering station, connected it to the same simple switch and I can ping the Windows server. On my Engineering station I have Simatic Manager with my integrated project. I open the project and try to download the WinCC project I get told that there is no connection to the RT project (that is true since there is no project yet on the Windows server). So what am I doing wrong and what is the correct way to download the wholde project to my new (replacement) WinCC server? AttachmentOMS.zip (23 Downloads) |
8/5/2019 11:13 AM | |
Joined: 9/30/2016 Last visit: 5/23/2024 Posts: 912 Rating: (6) |
Hi Georg, Thank you for answering. It is not a completely new project I want to download to the new server. It is a "old" WinCC 7.0 project that I have just migrated to WinCC 7.4 Upd. 1. So the fields in your screenshot is already filled out. Do I need to change those settings? On the now running (Win 7 and WinCC 7.0) server the project is placed in C:\WinCC Projekt\KALEC01SERV01 On the new (Windows Server 2012 and WinCC 7.4 Upd. 1) the project should be placed in D:\WinCC\KALEC01SERV01 Is this something I need to set up in the WinCC project and if so where? If the location of the WinCC project is NOT set up in WinCC how does the Enginering station know where to place the WinCC project?
AttachmentOMS WCC.zip (33 Downloads) |
Follow us on