11/9/2021 12:05 PM | |
Joined: 5/2/2019 Last visit: 1/3/2024 Posts: 37 Rating: (0) |
Now I can revive this topic. Instead of getting data from the excel I mentioned at the beginning, I can adjust where the actuators should go according to the values I give myself. It's a farm machine and it's scattering manure on the field. The speed of the tractor is detected by a GPS receiver sensor. The operator determines the amount of fertilizer he wants to apply and how many meters wide he will scatter. Related location LOGO! and guides the actuators to the correct position. There is also a calibration menu suitable for different fertilizer types. The program is a bit complicated but works very well in the field. I need to improve this job a bit and I'm working on it. Global fertilizer companies have created some programs to apply different amounts of fertilizer to different areas before going to the field. The farmer determines the desired amount of fertilizer for the locations and saves it as a shapefile or KML file. When he goes to the field, he starts the application by turning on his mobile phone. The application transmits the amount of fertilizer corresponding to the current position to the controller. In addition, we can get instant speed information from the mobile phone. (We are getting support on Android so that the tablet can transmit over Modbus TCP/IP) The part I don't know; What are the settings I need to do when receiving data over Modbus TCP/IP? I need to get B087 V1 and B010 V1 values via Modbus. First of all, I need to convert the attached program to "Network Project". Then I will add a "ModBus-Compatible device" and enter the IP settings. I don't know how to fill in the data transfer part from now on. Can you help me? You can also access the presentation of the application that adjusts the amount of fertilizer I mentioned above from the link. https://www.youtube.com/watch?v=ficvfTrMHno&t=2s ------------------------------------------------------------------------------------------
AttachmentHiza duyarlı GSM.zip (428 Downloads) |
Last edited by: Jen_Moderator at: 11/10/2021 08:58:39New subject after splitting. Edited text for better reading. Embedded video. |
|
Follow us on