Industry Online Support
Technical Forum
8/28/2014 11:42 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928) |
Hello guys PCS7 7.1 Redundant servers On one server we have a server fault. The servers can be switched over and client will also find the master server. I want to know what can cause the server fault error-> Internal WinCC tag: RedundantServerState I have seen that in the logfile, there are tags which have a incorrect format between AS and OS I have seen that for one PLC program in the multiproject, the netpro connection is only made to server 1 and not server 2. Could any of the two problems can set the server to fault state? |
If I could help you, you can use the RATE button. Thank you. |
|
11/24/2014 6:56 AM | |
Posts: 1 Rating: (0) |
Thanks for sharing. good luck |
Follow us on