9/12/2014 9:26 AM | |
Joined: 4/24/2006 Last visit: 11/18/2024 Posts: 8770 Rating: (1171)
|
Hello, Is it right, you can not even compile the project? Are you using the latest update for WinCC flexible 2008 SP3? Update for WinCC flexible 2008 Service Pack 3 Best regards, Wizard |
This contribution was helpful to2 thankful Users |
12/19/2014 4:58 PM | |
Posts: 56 Rating: (1) |
The issue was that that particular modelHMI didn't seem to support simulation. I do not remember which HMI it was though. |
12/19/2014 9:12 PM | |
Posts: 8946 Rating: (999) |
OP77B allows RT - Simulation. Please answer Wizard's questions. |
This contribution was helpful to2 thankful Users |
12/20/2014 10:57 AM | |
Joined: 1/21/2013 Last visit: 10/23/2024 Posts: 4620 Rating: (708) |
Hello gdglisch82, Are you sure you have WinCC Flexible 2008? Strange, I have one PC with WinCC Flexible 2008 without SP and I simulate the OP77B Why can't you simulate the Runtime for an OP73/OP73micro/TP177A/ TP177micro or OP77A in WinCC flexible on a PC? |
Last edited by: Ste39 at: 12/20/2014 10:58 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on