Industry Online Support
Technical Forum
1/14/2012 6:36 PM | |
Posts: 4 Rating: (0) |
What is Bico Technology? please explai in brief |
Last edited by: O_Moderator at: 1/16/2012 11:20 AMnew subject after splitting from /tf/WW/en/Posts/67952#top |
|
1/22/2012 1:01 PM | |
Posts: 116 Rating: (7) |
Hi, see manual http://support.automation.siemens.com/WW/view/en/49084671 chapter 12.4 Every drive contains a large number of interconnectable input and output variables andinternal control variables. BICO technology (Binector Connector Technology) allows the drive to be adapted to a wide variety of conditions.Digital and analog signals, which can be interconnected as required by means of BICOparameters, are identified by the prefix BI, BO, CI, or CO in their parameter name. For much more comfortable configuration use DCC http://support.automation.siemens.com/WW/view/en/49615426 Drive Control Chart (DCC) for SINAMICS (...and SIMOTION) means graphic configuration and expansion of the device functionality by means of freely available control, calculation and logic blocks
|
Follow us on