6/12/2013 10:53 PM | |
Joined: 9/27/2006 Last visit: 11/4/2024 Posts: 12293 Rating: (2690) |
Hello duy; Modbus RTU is Modbus RTU, and the mechanisms for implementing it on both platforms are very similar. Both the CP 341 (RS 485) and the 1SI can support up to 32 remote slaves, and the blocks for send/recieve on the Modbus protocol are very similar. Look at the following article exolaining the differences between the platforms: Which hardware and software components do you need to establish communication between SIMATIC S7 stations and third-party devices using the MODBUS RTU protocol? |
10/2/2024 9:34 AM | |
Joined: 10/1/2024 Last visit: 10/8/2024 Posts: 2 Rating: (0) |
Hi dchartier, Great questions!
To make the best decision, consider working with a lead generation company that specializes in automation solutions. They can help you explore your options effectively. Hope this helps! |
Last edited by: AutoGen_7115267 at: 10/02/2024 09:47:25Last edited by: AutoGen_7115267 at: 10/02/2024 09:49:43Last edited by: AutoGen_7115267 at: 10/03/2024 10:23:21 |
|
Follow us on