6/30/2023 10:26 AM | |
Joined: 6/30/2023 Last visit: 7/3/2024 Posts: 1 Rating: (0) |
Hello! What is the case with communication to redundant AS? Is it required to use Softnet Redconnect license (eg: SOFTNET-IE S7 REDCONNECT V16 / 6GK1704-0HB16-0AA0) to set up the Plantbus communication to 2 redundant AS (2xCPU410-5H + 2xCP443-1 on a bundle) from 2 ordinary/non Siemens PCs (ES/OS and OS stations) which aren't equipped with CP1623? Even when the number of CPU connections are within their limit, BCE or Softnet Lean or Softnet licences are not sufficient, right? best regards Kristof ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 06/30/2023 11:51:30New subject after splitting Last edited by: KristofNagy at: 06/30/2023 12:23:46 |
|
Follow us on