7/10/2023 3:51 PM | |
Joined: 3/14/2008 Last visit: 7/25/2024 Posts: 2079 Rating:
|
Hi, These are just the block versions used in SCL. With each update, the version is updated in the SCL source (used by development). They do not align always with a PCS7 version. Additionally, since V9.1, the block number, version, comment and other are also included as structure in the block itself so it's visible in CFC as well (if you unhide the structure). |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on