4/26/2022 12:39 PM | |
Joined: 10/2/2020 Last visit: 11/12/2022 Posts: 15 Rating: (0) |
i am in misery I have 6 Red Rack with AI, DI, and DO Cards to number 23 cards in total. My version is 8.2. So until the setting of the Redundant card to Twenty-first, I did not have any problem. But when I set the redundant setting for twenty-second card the size of FC767 rich up to 64K An error appears. This is very joking but hold my project. thank you
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/27/2022 09:05:58New subject after splitting |
|
5/4/2022 10:52 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (171) |
Closed cause question posted twice. The second thread with the subject Maximum length of area code reached (64 kb) is published within the conference Process Control Systems SIMATIC PCS 7. Jen_Moderator |
Follow us on