11/15/2019 9:08 PM | |
Posts: 30 Rating:
|
hello , I have redundant system.Server a and server b. server b master , sever a standby ; in server b when the pictures(in the graphics designer) is changes ,then at the any client ,I can see changes. Problem : when the server a is master and server b is standy , I can't see picture changes. How can I synchronize server a with server b, Thank you photo attached ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/18/2019 06:00:58New subject after splitting |
|
11/16/2019 3:09 PM | |
Joined: 9/9/2015 Last visit: 7/24/2024 Posts: 727 Rating:
|
Dear Hasan61, When you change the graphics in Server B, the station project picture folder graphics have been changed. wincproj\SERVER\GraCS\ xxx.pdl. This picture will not be synchronized with the folder in ES or Server A. You have to manually copy that picture files and paste it in the Server A wincproj\SERVER\GraCS\ xxx.pdl. Then you should also copy it in the ES folder as well, if not, when you do OS download later, the old pdl will override the new one in the SERVER A and SERVER B. Hope it helps. If you need more clarifications, do ask. |
Last edited by: JazTai at: 11/16/2019 15:09:46Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
1 thankful Users |
Follow us on