4/25/2019 3:25 PM | |
Posts: 2 Rating: (0) |
I have a Simatic S7-200 I need to access. Where can I get the Micro/Win software? I do have Step 7 V5.4 SP3. Is there a service pack available to access the S7-200? ------------------------------------------------------------------------------------------ |
Last edited by: Ron K at: 04/25/2019 17:01:33Last edited by: The Helping Hand at: 04/26/2019 07:21:20New subject after splitting |
|
4/25/2019 5:14 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (208) |
Depend on the program there is another way, just change the old S7-200 by a new Logo8. Anytime the old hardware will be defect, then you have the next problem to get spare parts. Regards, Scorp To buy the original software see also Link If the Link not work, then search directly for 6ES7810-2CC03-0YX0 |
Last edited by: Scorp at: 04/25/2019 17:15:17Last edited by: Scorp at: 04/25/2019 19:52:11 |
|
4/29/2019 7:07 AM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (208) |
As i have written some days ago there is no need to contact Siemens for special offers or to buy an old pg. You can buy the original software as spare part up to year 2025, see Link If the Link not work, then search directly for 6ES7810-2CC03-0YX0 in the Siemens mall. Regards, Scorp |
This contribution was helpful to1 thankful Users |
12/12/2020 11:16 PM | |
Joined: 9/27/2006 Last visit: 10/17/2024 Posts: 12289 Rating: (2687) |
Hello Rinor; The link you provide only allows the download of SP8 and SP9 for S7-MicroWin 4.0. To install these service packs, you need to have a previous installation of MicroWin v4.0 and the accepted Windows OS. You can still purchase MicroWin v4.0 (including SP8 and SP9) from Siemens, with the part number proposed earlier by Scorp: https://mall.industry.siemens.com/mall/en/ww/Catalog/Product/6ES7810-2CC03-0YX0 Contact your nearest Siemens rep to find out price and availability. Hope this helps, |
Follow us on