2/27/2023 2:42 PM | |
Joined: 8/15/2021 Last visit: 2/27/2023 Posts: 1 Rating: (0) |
Total DI - 38 DO - 28 AO -7 AI - 12 RTD -12 Shall i possibale to use S1215C PLC? If not then which model is comfartable? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/28/2023 10:17:05New subject after splitting |
|
2/28/2023 11:58 AM | |
Joined: 7/19/2022 Last visit: 4/26/2024 Posts: 356 Rating: (60) |
Hi qazsx, The technical data of the previous one is also useful: CPU 1215C, AC/DC/RLY, 14DI/10DO/2AI/2AO because there you can see which ones are integrated and how many expansion modules you can put in the S7-1200 (up to 8) to cover your needs. I would also recommend that for this type of configuration you use the tia selection tool: TIA Slection Tool where you can select the CPU and indicate how many inputs and outputs it needs to see the necessary components.
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on