11/27/2018 7:49 AM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating:
|
Please also see the screenshots. I need to install a WinCC 7.0 SP3 Upd. 1 client on a Windeows server 2008 PC. I need to make it as a replacement to a WinCC 7.0 SP3 Upd. 1 client that is running on Windows 8 Ultimate. The "old" client is still running (and in use so it must not be ruined until the replacement is ready) so I might check some options if really needed (one of the included screenshots in from the "installed programs on the "old" client). So - which options do I pick (which boxes in the screenshots do I check) to make a functional replacement of the client? And as a bonus question - how do I browse to the project on the server - where do I enter the IP-address of the server or how is it entered? AttachmentWCCC.zip (28 Downloads) |
Last edited by: xmnj at: 11/28/2018 9:27:47 AMLast edited by: xmnj at: 11/28/2018 2:12:23 PM |
|
11/29/2018 12:50 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating:
|
Hi, 1. You should check if the software is compatible with the compatool: https://support.industry.siemens.com/kompatool/pages/main/index.jsf 2. You shoud install the software on your new compatible system. 3. You can duplicate the project from your old system to the new system with the Project Duplicator. You should only activate one Network Card and look that a compatible version of SIMATIC Net is installed: https://support.industry.siemens.com/kompatool/pages/main/index.jsf B.R. |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on