4/29/2016 11:35 AM | |
Posts: 107 Rating: (20) |
I understand that you have HMI prjects and you need to access them on your PC. First you can try to download Wincc Flexible Trial version to check accessing your project. If you succeded, then you have to order original licensed one. |
4/29/2016 8:04 PM | |
Joined: 9/7/2007 Last visit: 10/9/2024 Posts: 550 Rating: (62) |
Hi Wirsan There are many software for HMI and you need to have the configuration file first so that you can open or edit it, else you can only take an image of the HMI and download it to another one with the same part number. If you do not have this Configuration file you do not need to get the HMI software
|
Best Regards |
|
This contribution was helpful to1 thankful Users |
5/1/2016 7:46 AM | |
Joined: 5/28/2008 Last visit: 10/12/2024 Posts: 4515 Rating: (839)
|
Hello Wirsan,
Hope this helps.
|
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
5/1/2016 8:22 AM | |
Posts: 8 Rating: (0) |
Hello Ayman Elotaify. Thanks for the quick answer! I will do the recommended options. Sincerely, Wirsan. |
Follow us on