1/18/2011 12:17 PM | |
Posts: 34 Rating: (2) |
In my project there are 4 servo motors,Simotion D425 and Sinamics drives. In my old Simotion Scout project Frame / base time is 0.250 ms.(see attachments) Without any change in configuration (same drives, same motors and same Simotion D425) I have made Automatic configuration for Sinamics and some changes in MMC programs. When I check Frame / base time I saw that it is 0.125 ms. Why? What is the effect of this value. I am trying to find out why new one is slower than old one? OPC communication is not good as old one. Attachmentattach.zip (328 Downloads) |
Follow us on