7/13/2017 5:29 AM | |
Joined: 3/10/2017 Last visit: 3/25/2024 Posts: 2 Rating:
|
Hello experts. I'm working with a simotion D 425-2 DP/PN with sinamics integrated, in a steel machine, but when the steel stuck on the knifes the simotion CPU goes to stop mode, I don't understand why is the reason for that.. Diagnostic buffer indicates that: 40202 dynamic response, this set on the axis when the knife cuts the steel. 50009 hardware limit switch, (when the microswitch isn't reached, but I can't acknowledge when this alarm is presented) and my processor goes to stop mode. once time reached these alarms I can't acknowledge until I restart the system turn off/on to simomtion and pass the selector mode to stop mode (number two) and return to run mode (number 0) There is a form that I can pass my proccesor to run trought a comfort panel 400? Thanks, I hope you can help me please, Best regards.. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/13/2017 12:02:28 PMNew subject after splitting |
|
Follow us on