1/13/2011 10:11 PM | |
Joined: 12/14/2010 Last visit: 6/28/2023 Posts: 160 Rating: (6) |
Greetings Bizur [schnippschnapp] Allow me to ask you a question on a doubt that I have a while ago, why I cannot consent to the configuration of the CCAgent for the way that siemens suggests ?, "Control Panel\WinCC Projects\Configuration" or by the "task bar -> rigth click->...." , in my system such ways don't appear, , only the Simatic Shell is shown in the Windows explorer tree, it is necessary to have the WinCC option NetCC ? best regards Splitted from WinCC- AP Connect failed, Error.................. |
Last edited by: O_Moderator at: 1/17/2011 8:30 AMnew subject after splitting |
|
1/18/2011 8:20 AM | |
Posts: 799 Rating: (43) |
hi jm1983, can you upload a screenshot of your system where something is missing in the task bar? Would be helpful! best regards |
1/19/2011 7:25 AM | |
Posts: 799 Rating: (43) |
dear jm1983, have you checked, if "CCAgent.exe" is running in task manager? I guess, that there is maybe an installation problem on your system. best regards |
Follow us on