6/21/2016 11:45 AM | |
Joined: 3/27/2012 Last visit: 7/22/2024 Posts: 179 Rating: (4) |
Hello Experts, I have a question about usage of Memory Card on CPU226 (and maybe others) We have alot of CPU200's on site and some of them works with Memory Card fitted on them and some Not. I Know that Memory card usage depends on the size of the program and also how we save parameters and so on ... I attached 2 project that one of them with Memory Card and the other one without Memory Card, project size for the one without Memory card is bigger than the other one and also we are not saving anything permanent on Memory Card and the structure of the projects are very similar! I can turn the power OFF-ON on the one without Memory card and project works as usual but on the one with Memory Card (fitted from start by the programmer), I can do the same if Memory Card is in its slot but if I pull out the Memory Card and then power it up the system won't work and this is the question I have " Why it doesn't work without Memory Card " The only different I see now is the Version of the PLC's, With Memory is Version 1.02 and without Memory is Version 2.01 Is That could be the reason for Memory Card??? Thanks There are 2 attachment, one here and one after this AttachmentWith Memory.zip (276 Downloads) |
Last edited by: AhooraJafari at: 6/21/2016 12:53:41 PMLast edited by: AhooraJafari at: 6/21/2016 12:57:28 PM |
|
6/21/2016 11:46 AM | |
Joined: 3/27/2012 Last visit: 7/22/2024 Posts: 179 Rating: (4) |
Belong to previous comment Both attachment work OK but for different machines. Thanks AttachmentNo Memory Card.zip (301 Downloads) |
Last edited by: AhooraJafari at: 6/21/2016 11:49:26 AM |
|
Follow us on