11/19/2010 5:55 AM | |
Joined: 1/28/2009 Last visit: 7/15/2024 Posts: 6844 Rating: (1363) |
Dear member Check this postfor same point. FB can be used as a static parameter of another FB. May it help to reduce generation of extra DBs?
|
This contribution was helpful to1 thankful Users |
11/19/2010 10:31 AM | |
Posts: 141 Rating: (0) |
Then why I cant do wit hte first way in ladder, why doesnt ladder like it (type check error)? |
11/20/2010 4:50 AM | |
Joined: 10/7/2005 Last visit: 7/20/2024 Posts: 3009 Rating: (1053)
|
another way is to simply drag the (S)FB from the (S)FB Blocks folder (or library), right mouse click on it and select "Change to Multiple Instance Call.." from the menu (note that this menu item is only available for (S)FB's that have call parameters). I hope this helps |
Cheers |
|
11/21/2010 2:43 PM | |
Joined: 1/28/2009 Last visit: 7/15/2024 Posts: 6844 Rating: (1363) |
Dear Goran_ Please check following link for detailed and illustrative disscusion on How do you create and update multiple instances? regards |
Follow us on