6/28/2011 12:19 AM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365) |
Check the following link for list of available communication drivers available in WINCC 7. You have option of using OPCs which are available to help like: http://www.matrikonopc.com/opc-drivers/opc-ge-plc-fanuc/base-driver-details.aspx You can also check documents of HMI software such as CIMPLICITY or IFIX which are originally developed by GE which I think the drivers embeded in the software! regards |
6/28/2011 5:59 PM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365) |
1-Why do not use CIMPLICITY which drivers of mentioned PLCs are available and embeded in the Software. 2-If you are familliar with WINCC and prefer to use it,You should have SIMATIC NET-OPC SCOUT and for example Matricon OPC server.OPC server provides data for OPC SCOUT and it can be used in wincc as discussed here. connect with the winccif you are interested in testing the most complex configuration and if you have all software packages, you can also use the Demo version of Matrikon OPC Regards Attachmentopc2wincc.zip (263 Downloads) |
6/29/2011 9:27 AM | |
Joined: 1/28/2009 Last visit: 10/11/2024 Posts: 6852 Rating: (1365) |
If you are familliar with industrial softwares, It is not ver difficult to handle. Check the following manuals: SIMATIC NET Industrial Communication with PG/PC Volume 1 - Basics System Manual Industrial Communication with PG/PC Regards |
Follow us on