1/13/2017 11:41 AM | |
Posts: 2 Rating: (0) |
Hello, I have a similar problem with Alarm Logging as MxStone. After power failure I do not see acknowledged alarms which are still active. If I forced alarm in the PLC to "0" then trigger it again to "1" it will show on the alarm list. I tried to fix it, but:
"For each message (rightclick - Properties) you have to check the option "will be archived" " - I do not have this option in tag properties I cannot choose option "Reload after power failure" as well - it is grey (disabled). I am using WinCC v7.3 upd 1. In the Alarm Logging I have: Message Class -> Message Type (where we have defined internal acknowledgment tag) -> Alarms into message type (each alarm has defined "message tag" from the PLC and parameter "archived" is checked). So each alarm uses acknowledged tag from message type. How can I fix it? Maybe at least is some possibility to reload manually all alarms. for example to force WinCC to check again all alarms? (compile all and download is not helping) Thanks for any help. Rafal ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/13/2017 12:49:26 PMNew subject after splitting |
|
1/13/2017 1:54 PM | |
Posts: 2 Rating: (0) |
Hello bg2492, Ok, I have checked this box. But what can I do with my issue? How can I show again all active alarms? Besr Regards, Rafal |
Follow us on