12/22/2008 4:12 PM | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating:
|
Hello markallinson , YES !!! and NO !!! you can project the MP 270 Bwith WinCC flexible but not the MP 270 Here is any help about migrating protool in Wcf: first a FAQ: http://support.automation.siemens.com/WW/view/de/18796902 and a short discription to your problem: (Sorry but you have to look for many things... Migration depending on the HMI You can basically migrate all ProTool projects created for graphic devices or Windows-based systems to WinCC flexible projects. The project must be available as a ProTool project file (*.pdb, *.pdz) to allow its migration. In the following cases, you require a ProTool engineering station to restore the project prior to migration:
Scope of migration The scope of migration depends on the HMI device you want to use to run the project:
Migrating ProTool projects with ProAgent elements Install the ProAgent option prior to migrating ProTool projects with ProAgent elements. Start the corresponding customized installation. Overview The tables below show:
Optimizing the HMI change The conversion quality depends on the degree of difference between the HMI of the ProTool project and the HMI of the WinCC flexible project. Certain differences between the devices, such as the number of keys, dimensions of the devices or performance classes, can be compensated by editing the converted project. Other differences may restrict the functionality of the converted project, such as scope of functions, data volume or performance. The tables below show:
Find the ProTool HMIs in the columns, and the WinCC flexible HMIs in the rows. HMIs with keyboard
here the discription:
I hope that i could help you.... |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||
Follow us on