11/2/2022 10:25 AM | |
Joined: 2/17/2020 Last visit: 10/9/2024 Posts: 1079 Rating: (192) |
Hi Mats_J, Perhaps these two FAQs help narrow down the problem: How do you set up Autostart for WinCC? How do you avoid synchronization problems with the Autostart of WinCC Runtime V7? Also, if the project is started manually, does the same thing happen or not? |
A rating will be well appreciated. |
|
11/2/2022 4:08 PM | |
Joined: 6/16/2015 Last visit: 10/7/2024 Posts: 21 Rating: (0) |
Hi Please notice it's not the time it takes to start WinCC and activating the project i talking about. It's the time after logged into windows and the long delay before the SIemens AutoStart even start up WinCC and begin loading the project I mean.
|
7/19/2023 12:42 AM | |
Joined: 9/9/2015 Last visit: 10/8/2024 Posts: 727 Rating: (278) |
I agree to the windows that inform the user that the wincc application will be starting. The delay of the autostart windows are too long. This gives an argument opportunity to end users to raise a cybersecurity concern where the operator can actually do something on the windows before the wincc runtime started. For our project, we are forced to implement a lot of hardening measure to avoid operator exit system during the boot up and wincc start up process. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on