12/22/2015 9:48 AM | |
Joined: 9/30/2013 Last visit: 8/23/2024 Posts: 7 Rating:
|
Hello Guys,
I have a problem regarding opening of WinCC project in WinCC explorer. When I click on the project file with .mcp extension, then I get the following error. The configured server is not available. Do you want to open the project using the local computer as the server? When I click on Start server locally then the project does not open and there is no error pop-up also. I don't know what's wrong with it. Earlier I had stopped the SQL service WinCC and mad a copy of the project folder the same local drive with a different name. After that I had tried to rename my original project but it said that this project is shared and renaming will cause the project to be unshared. So I did not rename my project. After that it stopped opening the project.
Please help! ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 12/22/2015 10:45:15 AMNew subject after splitting |
|
12/13/2018 9:43 PM | |
Posts: 14 Rating:
|
hi, friend, can you tell me how to solve this probpem? is it related to the nerwork environment you proposed? thanks for trainging furtherly. |
Follow us on