Industry Online Support
Technical Forum
2/15/2013 2:27 PM | |
Joined: 5/13/2008 Last visit: 12/18/2019 Posts: 836 Rating: (71) |
Hi Enock, an excerpt from the brochure: ... The reporting uses standard HTML that you can access automatically via email or FTP transfer, or on-demand via the integrated web server. The stored data fi les are also remotely accessible by FTP server. The FTP Push function sends data fi les to any remote FTP server for integration into your logistics systems. ... So it looks like, the only way to get the data into a WinCC RT is, to configure the WinCC PC as a FTP server, to get the HTML based reports. These reports can then read out via scripting from the WinCC RT. A direct data connection to WinCC RT (e.g. OPC) will not be supported by the RD500. |
mfG / Best regards |
|
Follow us on