12/10/2020 8:23 PM | |
Joined: 9/23/2005 Last visit: 8/27/2024 Posts: 4347 Rating: (1442)
|
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Switches are simple elements that allow the operator to alternately assign one of two values (e.g. true or false) to a variable. In addition to the assignment, it also clearly represents the status of this variable. Configuration: The assignment of values to the switch is done in the General -> Alternative state property. Tips:
Project (archived and zipped) AttachmentSwitch.zip (838 Downloads) |
Denilson Pegaia |
|
Follow us on