5/25/2015 4:19 PM | |
Joined: 9/3/2008 Last visit: 5/21/2024 Posts: 921 Rating: (158) |
Also make sure Simatic Net itself has been installed. I often encounter people overlook/forget this point. And about setting the PG / PC Interface, see the following link explaining it for WinCC 7.x. It is basically the same for WinCC Professional: How do you set the PG/PC interface with a TCP/IP connection in the S7 Protocol Suite? |
Michael |
|
5/25/2015 5:06 PM | |
Joined: 5/12/2006 Last visit: 5/14/2024 Posts: 22251 Rating: (2985) |
for winCC V13 you do not need a Simatic Net INstallation! This only need if you use WinCC V7.x! |
Follow us on