8/6/2015 10:52 PM | |
Joined: 2/18/2015 Last visit: 1/16/2024 Posts: 66 Rating:
|
Hello I'm working with Wincc Explorer V7.0. In this SCADA is only possible to create up to 2048 external tags due to the license. My problem is that I have few tags remaining, and I need more to go forward in my project. Although an update could figure out this, it isn't possible because of my client requirements. So, I'm thinking about using arrays in order to take up less tags; however, I realized that I can't created arrays as external tags. I wondering if someone knows how to make an array as an external tag or something similar to help me.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 8/7/2015 12:58:43 PMNew subject after splitting |
|
8/25/2015 1:32 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
New question published by gabbar is split to a separate thread with the subject WinCC v7.0 sp2, which licensed version for WinCC archive. Best regards |
Follow us on