8/2/2017 9:00 AM | |
Posts: 20 Rating: (2) |
Hi, I have connected my IoT2040 to the internet through a usb-wifi adapter .Should i change the ip address of the IoT (now it is the default 192.168.200.1). to the ip adress of the wi-fi so my iot 2040 can communicate with my PC wireless.If so how can i do that? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/2/2017 1:49:59 PMNew subject after splitting |
|
8/2/2017 10:57 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (379)
|
Hi, no you won't have to change the default IP address of 192.168.200.1 to have connection to you WIFI network. This IP address is set for the LAN interface eth0 (left ethernet port of an IOT2040). If you are adding a USB-WIFI dongle it creates an own network interfaces called wlan0. You have to use this one for the connection to your WIFI router. How to do this is described here. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
1/12/2018 10:20 AM | |
Posts: 10 Rating: (0) |
Is it possible to bridge the eth0 and wlan0 networks? |
Follow us on