11/14/2023 11:51 AM | |
Joined: 8/22/2021 Last visit: 12/2/2024 Posts: 11 Rating:
|
I am trying to understand the LOGO! CIM module but I keep running into problems. I have several projects working with a universal RTU-2 TCP gateway. One of these projects is a relay card that I want to control with a Logo! But now with the CIM module. In the Logo! I create a marker (flag), or output or a network output high. This I want to write away in the UDM register of the CIM. Then I want to read it out via restful api. Once written away in the UDM register I want to send it further to the RS485 relay card. But I am not that far yet. Transferring a word from the Logo! to the CIM is not a problem. I can read these out with restful API. Can someone help me? More information in the PDF Thanks AttachmentBit problem CIM module.pdf (390 Downloads) |
11/15/2023 3:39 PM | |
Joined: 8/22/2021 Last visit: 12/2/2024 Posts: 11 Rating:
|
After some experimentation, it worked. I got network output 10.1 working. Relay 1 of my RS485 device is now controlled. Still, I am curious to see how it works with a marker. I haven't managed that yet. In the attachment you can see what I did. Attachment15-11-2023.pdf (457 Downloads) |
Follow us on