1/19/2013 10:20 AM | |
Joined: 9/24/2010 Last visit: 8/6/2024 Posts: 27 Rating: (1) |
Dear all, I hope you get help as i have the same problem |
1/19/2013 9:05 PM | |
Joined: 3/14/2008 Last visit: 8/13/2024 Posts: 2084 Rating: (931) |
First try the Update block types function under options->Block types. It removes unused blocks from Blocks folder and CFC chart... Try again....Normally when you have blocks with different versions, the sytem should give you an screen where you can see the version and block that is already in CFC charts and the one you want to insert...Did you get that screen? Normally it would not be a problem
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
1/20/2013 3:38 PM | |
Posts: 35 Rating: (1) |
no i have not that screen. i deleted that block in CFC through right click on block and selecting delete but it seems this way is not correct |
1/20/2013 3:58 PM | |
Joined: 3/14/2008 Last visit: 8/13/2024 Posts: 2084 Rating: (931) |
You then just delete it from the CFC chart... if you check the library which says: Block program, it it still there... |
If I could help you, you can use the RATE button. Thank you. |
|
1/30/2014 11:20 AM | |
Joined: 9/1/2005 Last visit: 8/12/2024 Posts: 4104 Rating: (194) |
new questions published by ykemalbozare split to seperate threads with the subjects wrong block inserted - Insert V7.0 CFC block within PCS7 V8.0 and Unable to establish connection to module Stationmanager Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
Follow us on