5/28/2012 9:12 PM | |
Joined: 12/29/2011 Last visit: 8/9/2023 Posts: 39 Rating: (9) |
Is your control in Continuous path mode "G64" Mode or Exact Stop Mode "G60" when running the test programme with lots of small G1 moves? You can read up on this in Section 5.1 of the "840D Programming Manual Fundamentals" or click on the link below for this same section from DoconWeb. Path Action Explanation Also. The vibration while using the Handwheel could be relevant. Perhaps the Axis Positioning Gain is set very high, what values are in MD 32200 for X and Y Axis Please? Key sequence to reach them with the Service Password set is Menu Select-Start Up-Mach Data-Axis MD Use the Vertical Softkey Axis+ and Axis - to find X and Y. Best Regards Mr_al |
Follow us on