6/1/2014 8:04 AM | |
Posts: 114 Rating: (12) |
Hello Can i connect cp after Y-coupler Thanks in Advance
|
6/1/2014 8:11 AM | |
Joined: 6/8/2013 Last visit: 7/18/2024 Posts: 158 Rating: (9) |
Dear das, yes it is possible, but check bus. |
6/1/2014 8:30 AM |
|
Posts: 60 Rating: (8) |
HELLO, YES YOU CAN CONNECT.IS THERE ANY PROBLEM ARISE? |
6/1/2014 8:33 AM | |
Posts: 114 Rating: (12) |
Is it possible for cp-341 |
6/1/2014 9:01 AM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating: (306) |
HelloK C Das,
The question is, could you put the CP341 under a Y-Link in HW configuration?! The CP341 will require an ET200M. Siemens doesn't support ET200M after Y-Link. To work around this restriction, you could use a DPV0 ET200M GSD. Then you can put the ET200M under Y-Link but the bad news is that you won't find the CP341 in the DPV0 file. So, you should move your solution to ET200S or any other remote IOs that can operate under Y-Link. Best regards, H-H |
This contribution was helpful to2 thankful Users |
6/1/2014 9:42 AM | |
Posts: 72 Rating: (6) |
Also you have to check for max no of data transfer through Y link. |
6/1/2014 9:46 AM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating: (307) |
Hello K C Das
You can easily install the CP341 in a normal ET200M Rack ( With Redundant IMs ) so why Y-Link ? What is the communication protocol that you want to implement on CP 341 ? You can install ET200S downstream of a Y-Link and use 1SI CPs in the ET200S Rack. All ET200S CPs are permitted and they support almost all the communication protocols supported by CP341 ( Modbus / USS / ASCII / 3964R etc ). In fact In case of Modbus Master / Slave - you don't even need to buy expensive drivers as in CP341. The functionality is integrated in the CPs However you must remember thatthere is a limit of total I/O Area of 240 bytes each for Input and outputs for each Y-Link.( CPs can usually occupy8 / 16 / 32 bytes of address space ) Hope this helps Cheers Navnag |
Last edited by: Navnag at: 6/1/2014 9:51 AMThere is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
Follow us on