8/14/2021 4:01 PM | |
Joined: 4/5/2020 Last visit: 9/27/2023 Posts: 29 Rating:
|
Hi , i have tried this project but its not working and gave me an alarm "Component can't create object : ' File.Ctl.FileSystem " 25 ActiveX component can't create object: ' File.Ctl.FileSystem " , please need your help if you have an idea , bcz i am really needed to handle this , and see the below link its designed by Siemens Forum i downloaded https://support.industry.siemens.com/cs/ww/en/view/48015332 for both PC and Panel for the PC its fine but for the Panel gave me the same error as i mentioned above see the attached image Warm regard ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/16/2021 09:40:57Optimized link. Last edited by: Jen_Moderator at: 08/16/2021 09:43:20New subject after splitting |
|
8/27/2021 11:06 AM | |
Joined: 8/3/2009 Last visit: 6/25/2024 Posts: 13115 Rating:
|
Hello EDBSPW A WinCE Panel has different API Objects and funktions for File and FilesystemAccess than a PC based System. If you use the simulation then the PC based WinCC flexible RT is used for Simulation. The WinCE Functnio cannot be simulated on PC. They only can run on Panel itself. Here are some Information: Example for PC based: https://support.industry.siemens.com/cs/ww/en/view/26106418 Example for WinCE: https://support.industry.siemens.com/cs/ww/en/view/26107211 Some more information: https://support.industry.siemens.com/cs/ww/en/view/13408815 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on