12/20/2021 8:56 AM | |||
Joined: 12/15/2021 Last visit: 3/23/2022 Posts: 11 Rating:
|
Hello, I am new to PLC automation. I am having the same problem as with not getting access to the panel since, password was entered wrongly. I have tried the below steps to resolve the problem but i was not able to download the project to HMI panel. Here are the steps that i have done, I used a USB flash disk to backup my current project. I have created an empty new project in wincc flexible under user adminstration i set a new password. Complied the project and I used an ethernet cable connected with the my Laptop and Hmi panel. Now, in wincc flexible ,under project I have set to transfer, and transfer page pop up after sometime, it said connection does not estabilished and failed to transfer. I did not know where i made the mistake.
------------------------------------------------------------------------------------------ |
||
Last edited by: GowthamA at: 12/20/2021 09:08:02Last edited by: GowthamA at: 12/20/2021 13:53:51Last edited by: Jen_Moderator at: 12/20/2021 14:08:19New subject after splitting |
|||
1/5/2022 10:50 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hello, Perhaps the following links might help: How can you transfer a WinCC (TIA Portal) configuration to an operator panel using Ethernet? Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
1/5/2022 12:45 PM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating:
|
Hi, So you get a Backup using Prosave, how did you connect to the panel? Best regards, Wizard |
1/5/2022 2:14 PM | |
Joined: 12/15/2021 Last visit: 3/23/2022 Posts: 11 Rating:
|
Hello Mr.Wizard, I Used Ether net cable to connect my laptop with the panel. Thanks for the help. Gowtham |
Follow us on