12/4/2024 7:35 PM | |
Joined: 10/3/2022 Last visit: 1/15/2025 Posts: 1 Rating:
|
Hello everyone, I am facing the following issue: I have a Siemens Reyrolle IED configured as a Modbus server and an S7-1500 as the client. I need to read some analog values such as voltage, current, and power on my PLC. The Modbus TCP communication has been established, and I can successfully read the first value from address 30180 (the Modbus address in the Reyrolle relay). However, when I increase the number of registers to read (MB_Data_Len > 1), I do not receive any data in my array. Does anyone have any suggestions to help me resolve this? Thank you! AttachmentPrints_with_MB_DATA_LEN_1_and_Greater_than_1.zip (143 Downloads) |
Follow us on