7/23/2024 12:03 PM | |
Joined: 8/3/2009 Last visit: 9/12/2024 Posts: 13656 Rating: (1725) |
Hello jovepre In the manual of Scalanve 615 it is listed: https://support.industry.siemens.com/cs/ww/en/view/109964163/149746485387 But all example I can find are with MUM856... Bye Murof |
If this Information really helps, you could use the Rate function |
|
7/24/2024 6:22 AM | |
Joined: 4/19/2018 Last visit: 9/8/2024 Posts: 4 Rating: (0) |
Thank you Murof. Indeed, the manual of S615 lists the feature and the WBM shows the VXLAN config tab, but the same manual indicates, in the section "Available services", that VXLAN is "8) only available with the SCALANCE MUx85x." https://support.industry.siemens.com/cs/us/en/view/109964163/179138592395 I have been comparing the WBM of S615 (V8.1.0) vs SC646 (v3.1.0), and with the S615 is not possible to check the box to activate VXLAN. I don't figure out if it is an incompatible configuration with other feature that blocks VXLAN or the S615 is not really compatible and it is a confusion due the shared firmware with the SCALANCE M800. |
Last edited by: Wit_Moderator at: 07/25/2024 11:05:55Link optimized |
|
Follow us on