Industry Online Support
Technical Forum
12/5/2005 6:10 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, i make a screen shot from the STEP7 Hardware to transfer this to the PLC SIM. (PLC_SIM.gif) Are the PLC in "Run"? In flexible look to flexible "gif". When there are all OK, then you shout get a conncetion to PLC SIM. Maybe you have a installation problem. (Deinstall PLC SIM [:(]) and install it again) Check the PG/PC Interface (I think, it shout not be stand on "PC internal") Sorry, but this ia all what i can do. AttachmentPLC_SIM.zip (1095 Downloads) |
12/5/2005 8:41 PM | |
Posts: 9 Rating: (0) |
Thank you for pictures, it was very helpfull.
I have good connection but this connection is via Profibus. I'm student and I'm writing program for University and there is no profibus module (only S7-313 and I/O). That's why I need to connect via MPI. It is possible to have connection via MPI???
I make screenshot with my configuration. Do you know what I must change to have a connection via MPI?
AttachmentMYconf.zip (990 Downloads) |
Last edited by: bzykus at: 12/5/2005 8:43 PMLast edited by: bzykus at: 12/5/2005 8:42 PM |
|
12/6/2005 9:19 AM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, i will give you one information again.[:)] Make a double cklick on your CP5411. Then you can change your "Adress" -> MPI. Change your PG/PC Interface setting. You use ander the Access Point ...PPI -> This are, if you want to connect to a S7 200! Change this setting to Profibus/MPI ==> Go into your System Setting from your PC I make two screen shots. I think, this could be help. AttachmentNew.zip (1110 Downloads) |
Follow us on