Industry Online Support
Technical Forum
7/26/2014 10:36 AM | |
Joined: 1/21/2013 Last visit: 10/23/2024 Posts: 4620 Rating: (708) |
When the E-Stand is the same, can i use the Prosave file even if the two panels are different? I mean, the first panel is a monochrome panel and the second panel is a color panel, but the two panels are OP27. Hello Edercy, If you have different part number i don't think Please have a look: How can you determine the "E-Stand" (hardware release) of an operator panel? Very interesting thread for yourproblem: Replacement of the siemens Panel |
Last edited by: Ste39 at: 7/26/2014 10:49 AMLast edited by: Ste39 at: 7/26/2014 10:40 AMAdded Thread |
|
7/26/2014 9:21 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, it is not possible. Try to get the protool-file or the same panel (same order-no) Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
8/20/2014 8:56 PM | |
Posts: 4 Rating: (0) |
Thanks for your answers, i had to get the same panel again. Eder
|
Last edited by: Edercy at: 8/20/2014 8:58 PM |
|
Follow us on