4/4/2013 11:46 AM | |
Posts: 3037 Rating: (192)
|
Hello, Which number has the oldest and which the new OP27? /tf/WW/en/Posts/87186 Tweety How can you make a project backup from an operator panel? |
Last edited by: Tweety at: 4/4/2013 11:59 AM |
|
4/4/2013 5:47 PM | |
Joined: 8/22/2011 Last visit: 9/4/2024 Posts: 52 Rating: (0) |
Dear Mr. Tweety, the old op27 part number :6av3627-1jk00-0ax0 the new op27 part number: 6AV3627-1LK00-1AX0 |
4/5/2013 2:05 PM | |
Posts: 3037 Rating: (192)
|
Hello, You can check your backup restore with another PROSAVE version. ServiceTool ProSave V1.1 If the restore does not work, then you can start a Support Request. Tweety |
4/15/2013 8:10 AM | |
Joined: 5/28/2008 Last visit: 9/8/2024 Posts: 4515 Rating: (839) |
Hello, The difference between two panels are as follows:
So the two panels are not identical. To restore image, you should have the same part number of the original one. If you have the configration file, you can make conversion to the new panel and download project on it. Hope this helps.
|
Ayman Elotaify |
|
7/25/2014 9:47 PM | |
Joined: 4/5/2006 Last visit: 8/13/2023 Posts: 642 Rating: (131) |
Hello, sometimes you also have this problem when you have different E-Stand. Which order-no? Regards André Räppel --------------------------------------------------------------------------------- www.raeppel.de work faster withinnovative PLC-Tools |
7/26/2014 7:27 AM | |
Posts: 4 Rating: (0) |
When the E-Stand is the same, can i use the Prosave file even if the two panels are different? I mean, the first panel is a monochrome panel and the second panel is a color panel, but the two panels are OP27.
|
Last edited by: Edercy at: 7/26/2014 7:28 AM |
|
Follow us on