10/18/2022 7:36 AM | |
Joined: 2/17/2020 Last visit: 5/22/2024 Posts: 1005 Rating: (176) |
Hi thanozn, I have been reviewing information about it, and it seems that it is possible as of WinCC Unified (TIA Portal) V17 Update 4 and an image version V17 + Upd4 installed on the UCP (Unified Comfort Panel). SIMATIC HMI Unified Comfort Panels Control Panel V17 - Network drive Also, you can use system functions, such as 'Export tag log as CSV', to enter the path of the shared folder and thus copy the logs. Another option is to have a USB stick inserted in the CPU, select the USB as a path in the DataLog itself, and then use the "copy.sh" script to copy the logs from the USB to the shared folder. |
A rating will be well appreciated. |
|
This contribution was helpful to1 thankful Users |
Follow us on