10/2/2023 3:58 PM | |
Joined: 6/9/2021 Last visit: 6/14/2024 Posts: 21 Rating: (1) |
Hi, You still have the wrong image into the micro SD card? U should install the correct image from the following link: Downloads for SIMATIC IOT20x0 - ID: 109741799 - Industry Support Siemens To erase the wrong image from your SD u can use disk administrator of windows, or SD card formatter: SD Memory Card Formatter for Windows/Mac | SD Association (sdcard.org) After that follow this instructions to install the SO: Application description (gothightech.com) You should be able to connect via Putty with the ethernet interface of IoT. Default ip is 192.168.200.1 (interface 1) and port 22. Best regards, Javertz.
|
Follow us on