12/18/2023 7:08 PM | |
Joined: 12/18/2014 Last visit: 5/19/2024 Posts: 33062 Rating: (4083)
|
The LOGO! 6ED1052-1MD08-0BA1 with Firmware 1.83.02 is the current LOGO! 8.3, not a FS4_LOGO!.It is in the hardware selection a LOGO! 8.3. The coming LOGO! 8.4 has the order number 6ED1052-XXX08-0BA2 with Firmware 1.84.01 and is in the hardware selection a LOGO! 8.4. AttachmentVersions of 0BA8.txt (287 Downloads) |
12/18/2023 7:31 PM | |
Joined: 12/18/2014 Last visit: 5/19/2024 Posts: 33062 Rating: (4083)
|
I didn't write that. Of course the upcoming LOGO! 8.4 has innovations. And the firmware of a LOGO! 8.3 cannot be updated to the firmware of a LOGO! 8.4. See also this topic: New features in the coming LOGO! 8.4 |
12/18/2023 7:38 PM | |
Joined: 7/1/2023 Last visit: 5/15/2024 Posts: 67 Rating: (0) |
I should have been more clear - I said "update the hardware" when I should have said "replace the hardware" There is no advantage to simply update from LSC 8.3 to 8.4 unless I replace the BM 0801 to an 0BA2? What does the FS04 signify? In any case, I will be replacing the BM whenever I can get my hands on the new release |
12/18/2023 7:42 PM | |
Joined: 12/18/2014 Last visit: 5/19/2024 Posts: 33062 Rating: (4083)
|
See also this topic: Firmware version logic (FS:0x) |
Follow us on